Default Header
(header konnte nicht geladen werden)
5/30/2007 7:42 PM | |
Joined: 12/20/2005 Last visit: 8/27/2025 Posts: 79 Rating:
|
Hello MMAB, You will need the Ethernet version of 4-mation to do the programming and downloading. The Ethernet to MBUS interface is the IEM and it is not obsolete (the NIM and RNI are however). To make the connection from the IEM to the QUADLOG modulrac, you will need a pair of MBI cables and a Y-cable. The attached drawing may help... Good luck, RJP AttachmentIEM Gateway Rev3.pdf (1126 Downloads) |
Follow us on