Default Header
(header konnte nicht geladen werden)
5/23/2007 11:05 AM | |
Posts: 6 Rating:
|
Dear Expert The redundant system (CPU417-4H) with two FM 458-1DP modules, Both FM458 profibus is connected to ET200M (IM153-2) in redundant profibus configuration, is this configuration possible ? (in hardware config is possible) but how to control system redundancy on ET200M(IM153-2), in other words how to command the profibus slave(IM153-2) redundancy change over from FM458 ? May some think with life bit monitoring ? Hwconfig.pdf attached.
AttachmentHWconfig.pdf (1005 Downloads) |
Follow us on