Default Header
(header konnte nicht geladen werden)
7/8/2013 11:02 PM | |
Posts: 11 Rating:
|
I been trying to get data going from one node to another I have the ACM to ACM reads and writes working. But using the GW_READ and GW_WRITE is proving a problem The system currently has those working, but If I try and add another connection it will fault the ACM I have included a set of Nodes that I assigned to two different SIMs and the connection works, however no data seems to be working Can not figure it out, should be working Maybe someone who is better than me can take a look at the code To get it working using Control Simulator, create two SIM modules on your dest top Resoure Name :RL1_A Node 1 Rack 1 Slot 1 8 M Advanced Control Module x Resoure Name :RL2_A Node 2 Rack 1 Slot 1 8 M Advanced Control Module x then transfer off line resource to online resource SIM modules hope you can help Thanks AttachmentNODES.zip (775 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on