Default Header
(header konnte nicht geladen werden)
4/25/2014 10:53 AM | |
Joined: 8/31/2005 Last visit: 9/12/2025 Posts: 2198 Rating:
|
General you need no software to parametrate the inverters, you can use the operator panels, but I recommend to use a software tool. For the SINAMICS G120 you can use Starter or Startdrive. Both software tools use USB, PROFIBUS or PROFINET to communicate with the G120. If your "Simovert VC" is aMASTERDRIVE(with CUVC), then you can use DriveMonitor. It uses a serial interface (e.g. COM1) to commuicate to the MASTERDRIVE. Maybe this helps you with the MASTERDRIVE: http://www.industry.usa.siemens.com/drives/us/en/electric-drives/maturing-siemens-drives/masterdrives-from-siemens-industry/downloads/Documents/DRV-MasterDrives-DriveMonitor_docs.pdf |
|
|
This contribution was helpful to
2 thankful Users |
Follow us on