5/28/2014 7:35 PM | |
Posts: 2 Rating:
|
Hallo, wie kann ich die Touchoberfläche unter Windows 7 betreiben ? 6AV7861-2TB10-1AA0 Grüße Oliver |
5/28/2014 7:47 PM | |
Posts: 559 Rating:
|
Please post in English. |
5/28/2014 7:56 PM | |
Posts: 784 Rating:
|
Kindly check the type of panel monitor. |
5/28/2014 8:02 PM | |
Joined: 5/28/2008 Last visit: 9/3/2025 Posts: 4522 Rating:
|
Hello, Let me correct part number for you. It should be "6AV7861-2TB10-1AA0" This Flat Panel is a just touch panel with VGA interface and DVI interface. You need to connect it to a PC with VGA / DVI cable. Hope this helps.
|
Ayman Elotaify |
|
This contribution was helpful to
1 thankful Users |
5/28/2014 8:19 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
The issue is that specially for touch screen is using a USB cable. Info is there: Delivery Release: SIMATIC Flat Panel Monitors 17" and "Extended"And as you know for each kind of USB needs a drivers. Unfortunately officially the drivers which is comming with CD is for:
And now who has expirince with the same in case of Win7? Personally I would trySupport Request. ![]() Best regards, Hristo Mihalev
|
This contribution was helpful to
2 thankful Users |
3/20/2015 7:39 AM | |
Joined: 10/21/2011 Last visit: 11/7/2024 Posts: 10 Rating:
|
It may be useful to someone. You need to download and install the driver from the website http://www.elotouch.com/Support/Downloads/Driver/DriverDownload/Default.aspx I installed the driver who called Elo Touch Solutions Single-Touch Driver (version 5.5.3), |
Follow us on