11/3/2011 12:28 PM | |
Joined: 1/26/2011 Last visit: 11/12/2024 Posts: 243 Rating:
|
Hi, have you tried these two options on the pictures in the .zip-file before? 1. Repair the Network Connection 2. Roll Back Driver Some other user (standard Windows XP user with a normally Computer) have the same problem and on the Windows Website in the forum it says that they have to uninstall and install the driver. If this doesn't help than just take the Recovery CD from your IPC427C and run it. After the Recovery it have to work. Another last crazy idea is: Delete the CP 1616 from WinLC Place the IE General in the WinLC (on IF1 - IF4 dosen't matter) Reboot Delete IE General from WinLC Reboot And then try if you can change the IP Address Must be the same as to Reinstall the Driver. My problem hereis, that i can't reproduce your case. But if you have another idea or the solution for this problem, please let us know :) regards bigfoot AttachmentDriver Options.zip (541 Downloads) |
Last edited by: bigfoot at: 11/3/2011 12:29 PM |
|
This contribution was helpful to
2 thankful Users |
Follow us on