Default Header
(header konnte nicht geladen werden)
12/24/2007 11:07 AM | |
Posts: 137 Rating:
|
Hi all i need the manual which illustrates how can i make upload & download by using (BOP) for micromaster411 ... urgently best regard maher |
12/25/2007 9:38 AM | |
Joined: 3/4/2006 Last visit: 7/28/2025 Posts: 73 Rating:
|
I have never used the MM411 but looking at this the MM411 BOP looks similar to that of the MM420/440, in which case it would not have any memory to store parameter sets. Check this for the MM411 manuals. |
1/26/2008 8:39 PM | |
Posts: 39 Rating:
|
Hi maher, AOP is used specifically for the MM411.you can click and download the operation manual from here https://support.automation.siemens.com/WW/skm/pdfviewer.asp?HitsPerSite=50&ehbid=html_76%2Fehb%2F24545742%2Ehtm&lang=en&nodeid=24545451&query=MICROMASTER%20411&page=3&view=new Hope this will be helpful, Rubeen. |
Follow us on