10/26/2015 7:45 AM | |
Joined: 4/14/2010 Last visit: 6/26/2025 Posts: 525 Rating:
|
Greeting, We want to synch the speed of two geared motors of conveyors without slippage because precision require in a millimeter, there is one automatic engine supply conveyor between one engine assembly and one frame assembly as attached layout. Please suggest which type of motors and drives can done this Job..?? Geared Motor Specification: 0.37KW, Torque 1320Nm Output RPM 1.5 Regard's AttachmentAes conveyor.pdf (311 Downloads) |
MS |
|
10/26/2015 11:16 AM | |
Posts: 61 Rating:
|
Is that possible to adapt any kind of encoder? |
10/26/2015 1:15 PM | |
Joined: 11/29/2011 Last visit: 2/4/2025 Posts: 1362 Rating:
|
Hi, This example should help you: Browse for further examples here: https://www.automation.siemens.com/mc-app/sinamics-application-examples/ I hope I could help! |
Last edited by: MicroMan at: 10/26/2015 1:23:29 PM- What you read here, please check with manuals and your requirements. |
|
10/26/2015 2:33 PM | |
Joined: 4/14/2010 Last visit: 6/26/2025 Posts: 525 Rating:
|
Thanks MicroMan, As in attached schematic both motors are coupled with one belt but in our scenario both motors are independent with their conveyors, and both having different pitch from one gadget to another that's why we want to synchronizing the speed. according to above example in master slave concept, and if both motors having independent conveyors. 1. Will this work for Speed synchronizing with no Slippage (required precision in millimeter)..?? 2. Which kind of Geared Motor will be used..?? 3. Which type of encoder sensor will be used...?? 4. Is MM440 Suitable for Servo Geared Motors..??
|
Last edited by: Sarfraz Bhatti at: 10/27/2015 11:13:09 AMMS |
|
Follow us on