Default Header
(header konnte nicht geladen werden)
3/25/2008 9:05 AM | |
Posts: 3 Rating:
|
ahmetsen2006, Pardon me, but if Iread Your message correctly - it is SIMOREG DC MASTER, right? If yes, then noone here can help with the information You have provided - see, F033 is nothing but Your own user-defined fault which is programmed via U102.01, .02, .03 and .04 binnectors. Revise Simoreg Compendium and then revise what program You have downloaded to Simoreg - this program is creating the bits which make F033 via U102. At least, if speaking about Simoreg DC Master. BR, C-E-S Medium Voltage Team. |
Follow us on