4/23/2018 2:55 PM | |
Joined: 5/12/2006 Last visit: 9/23/2025 Posts: 22691 Rating:
|
Hello, from the technical data: https://support.industry.siemens.com/cs/ww/en/view/87514778 Intel® HD Graphics Controller, P4600/P4700 GT1/GT2 Graphics Controller integrated in processor with three independent 2-D and 3-D Engines. • Intel® DH82C226 Express (Platform Controller Hub) – VGA: 2560 × 1600/32-bit color depth/120 Hz – DVI-D: 2048 × 1152/32-bit color depth/60 Hz – DisplayPort: 4096 × 2160/32-bit color depth/24Hz • Graphics memory: Up to 1.7 GB, used in system memory, 32 MB reserved. Multi-monitoring You can operate up to five monitors simultaneously at the interfaces of the integrated graphics controller in combination with the optional graphics card. Parameter assignment is performed by means of the Control Panel in Windows. The following monitors can be operated simultaneously on the motherboard: ● 2 × DisplayPort, 1 × DVI ● 2 × DisplayPort, 1 × VGA ● 1 × DisplayPort, 1 × DVI via DisplayPort-DVI adapter 1, 1 × DVI ● 1 × DisplayPort, 1 × VGA via DisplayPort-VGA adapter 1, 1 × VGA via DVI/VGA adapter 1 ● 1 × DVI via DisplayPort-DVI adapter, 1 × DVI via DisplayPort-DVI adapter 2, 1 × DVI ● 1 × VGA via DisplayPort-VGA adapter, 1 × VGA via DisplayPort-VGA adapter, 1 × VGA via DVI/VGA adapter 1 available as accessories 2 active DisplayPort-DVI adapter Detailed information is available in section "Accessories". Note The motherboard supports up to one additional DVI monitor if it is connected by means of a passive DisplayPort-DVI adapter. The additional Graphic card can be a NVIDIA NVS300/315 (This drivers are on the DVD), so i think is a DMS59 Interface which then use Adapters for DVI or VGA. Regards |
Last edited by: ChristophD at: 4/23/2018 3:24:24 PM |
|
This contribution was helpful to
1 thankful Users |
Follow us on