8/23/2018 1:05 AM | |
Posts: 1 Rating:
|
Hi all! I'm using a MicroMaster 420 to replace a old defective board from a industrial mixer like the one in attach. My problem is: The mixer has one POT and 2 NO momentary switches, one to start and the other to stop, and I can't figure out the way to configure the micromaster to run after click start once and stop after click stop, without using external relays. I search on the web and found some FAQ on siemens support showing the paremeters to do this (link is above) but some of the parameters didn't apear on my model (even in Lever4) - like "P2822" https://support.industry.siemens.com/cs/ww/en/view/41158384 Anyone knows if it is possible to do it in the Model -->420? PS. I bealive this is not a big deal to do, but i'm *** to this stuff and is my very first time using siemens Thank you all! |
Last edited by: Jen_Moderator at: 8/23/2018 9:43:27 AMOptimized link. |
|
Follow us on