Default Header
(header konnte nicht geladen werden)
11/29/2019 1:06 PM | |
Posts: 1 Rating:
|
How could i take 4-20mA analog from MM420 which option i have select in parameter list so drive AO signal is 4-20mA. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/29/2019 13:14:40New subject after splitting |
|
11/29/2019 4:53 PM | |
Joined: 7/19/2018 Last visit: 10/15/2020 Posts: 19 Rating:
|
Hi Parameters about Analog Outputs are from P770 P771 : Define function of 0-20 mA analog outputs P775 : Permite absolute value P776 Types of DAC P777 : Value x1 of DAC scaling P778 : Value y1 of DAC scaling P779 : Value x2 of DAC scaling P780 : Value y2 of DAC scaling For detailed explanation about parameters https://cache.industry.siemens.com/dl/files/275/24525275/att_82408/v1/420_PLi_24525275_en_1006.pdf at page 58 I hope helps you Best regards
Attachment420_PLi_24525275_en_1006.pdf (348 Downloads) |
Last edited by: Jen_Moderator at: 12/02/2019 07:44:07Added PDF file as an attachment. |
|
This contribution was helpful to
1 thankful Users |
Follow us on