2/24/2020 4:18 AM | |
Joined: 9/27/2006 Last visit: 9/11/2025 Posts: 12406 Rating:
|
Hello PaisPisco; Before current signals became a standard in control equipment, pneumatic networks were long used as input signals. Pneumatic signals were designated 3-15 psi levels, for analog ranges. The 3-15 psi range was selected so that if there was a break in a pneumatic tube and the system went to atmospheric pressure (0 psi) the system could produce an alarm, not a 0 signal. The same philosophy was used to design 4-20 mA electrical circuits. A wire break (open circuit) will generate a 0mA signal, which can be used for alarming. More information can be found in web articles such as this one; https://www.sensorsone.com/why-offset-4-20ma-3-15psi/ Hope this helps, |
This contribution was helpful to
1 thankful Users |
Follow us on