Default Header
(header konnte nicht geladen werden)
8/4/2020 11:51 PM | |
Joined: 7/13/2020 Last visit: 11/28/2024 Posts: 16 Rating:
|
I'm also trying to figure this out also. I'm creating a few dynamic symbols via faceplates and scripting, for example, a 3 pos selector switch, the problem is when I resize the faceplate on the screen the SVG graphics stay fixed size and don't resize with the faceplate when I do resize I just get the scroll bars to appear. I have tried all the different image modes such as stretch etc and tried faceplate in window and screen modes etc I just can't find a way to do this. I don't want to make a bunch of different face plates just to have different size symbols. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/05/2020 06:30:53New subject after splitting |
|
Follow us on