Default Header
(header konnte nicht geladen werden)
2/9/2009 5:17 PM | |
Posts: 102 Rating:
|
Dear Experts, I have backup of old 16bit SIMD rack. and need to recompile it. It sounds like the code contains some user define macro and the block name is CEPW1.B I also have USER0 directory backup which was used to generate this code. Can any one have look in this folder to identify that weather this folder contains this library or macro so that I can recompile the FB, FP and MP? I am attaching some library files. Please guide me. Dutta AttachmentUSER0.zip (528 Downloads) |
Follow us on