2/18/2021 9:33 PM | |
Joined: 12/13/2011 Last visit: 5/20/2025 Posts: 123 Rating:
|
It seems there was something wrong with my install :(. I will update once I have figured out the issue. |
4/19/2022 11:45 AM | |
Joined: 11/8/2019 Last visit: 12/23/2022 Posts: 1 Rating:
|
Do you know what went wrong? I have the same issue. |
9/26/2023 11:36 AM | |
Joined: 1/21/2013 Last visit: 8/29/2025 Posts: 4087 Rating:
|
Hi Jarb77, Do you have the WinCC Unified PC RT software installed? For WinCC Unified V18 this is no longer bundled with the TIA Portal software and must be installed separately. Kind regards |
9/26/2023 1:40 PM | |
Joined: 1/21/2013 Last visit: 8/29/2025 Posts: 4087 Rating:
|
Hi Jarb77, Yes, your screenshot shows that you have WinCC Unified PC RT software installed. However, since you have installed V18 Update 2 for the engineering software, I would recommend that you also install an update for WinCC Unified PC RT. When creating a configuration on your system, device version V18.0.0.2 is selected by default and to be honest, I am not sure if simulation will work with an older version of PC RT. You should also run the "WinCC Unified Configuration" to adapt your settings to your computer. You would have been asked to do this during the installation, but you are not forced to do it. If the PC RT is installed, your browser should display the WinCC Unified page when you access https://localhost or https://127.0.0.1. Note: Your browser may block the connection in this case because the certificate is created for your computer. Therefore, you must enter your computer name instead of localhost. When you view the details of the browser message, you should see the expected computer name. Kind regards |
9/28/2023 1:51 PM | |
Posts: 6 Rating:
|
Hello, Please find attached all the requested screen captures. I haven't stumbled upon any procedure related to the certificates. If you could point me to one, that would be very helpful. Thankyou! AttachmentScreenCaptures.zip (470 Downloads) |
Last edited by: Jarb77 at: 09/28/2023 13:53:16 |
|
3/25/2025 10:50 AM | |
Joined: 8/9/2013 Last visit: 3/25/2025 Posts: 2 Rating:
|
I encountered the same issue with TIA Portal V17 Update 8, where the Unified simulation would only bring up the extended download popup. After some digging, I found that this was a known issue with the V17 updates, and there’s a note about it on the download page. Installing the patch resolved the problem. This is something to keep in mind if you rely on TIA Administrator to keep everything up to date—it may not highlight important notes that impact critical features! Updates for STEP 7 V17, S7-PLCSIM V17 and WinCC V17 - ID: 109784441 - Industry Support Siemens Important notice - Effect on Unified PC Runtime and on RT simulation
|
Last edited by: Moderator_Lan at: 03/25/2025 10:59:22link optimized |
|
This contribution was helpful to
2 thankful Users |
Follow us on