1/9/2006 4:06 PM | |
Joined: 9/13/2005 Last visit: 11/18/2019 Posts: 86 Rating:
|
[quote user="burnett"] Hello, Hello Mr. Burnett! There is a very nice configuration example available as FAQ: http://support.automation.siemens.com/WW/view/en/19353091 This example is for PCS 7 V6.0 SP3a but most steps are still the same in V6.1!!! The only difference is that the "Commisioning wizard" mentioned in the FAQ is not available in PCS 7 V6.1 because it is no longer necessary, you can just leave out this step. |
Best Regards - Mit freundlichem Gruß - yoroshiku onegaisimasu - Sincères salutations |
|
Follow us on