1/22/2013 8:50 AM | |
Joined: 5/28/2008 Last visit: 8/6/2024 Posts: 4515 Rating: (838) |
No it is not available. This product "6AV3607-1JC20-0AX1" cancelled as from 1/10/2007.
No you can not use PPI cable. You have to use serial cable with pin assignment as follows. But keep in mind that you will be able to upload only an image file. Which means that this image is downloadable only on panels with the same part number. Hope this helps. |
Ayman Elotaify |
|
1/22/2013 11:01 AM | |
Posts: 7 Rating: (0) |
Sir thanks alot for ur prompt reply How can we go to transfer mode in OP7
|
10/7/2014 11:24 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4769 Rating: (123) |
|
8/6/2024 6:28 AM | |
Joined: 7/30/2024 Last visit: 8/8/2024 Posts: 71 Rating: (1) |
New question published by latent111 is split to a separate thread with the subject in the Module addresses in blocks and reference data is not displayed. Best regards |
Follow us on