3/4/2025 4:35 PM | |
Joined: 2/11/2015 Last visit: 9/9/2025 Posts: 512 Rating:
|
Ad. 1 - The FC36 not call inside. These properties shows the calls FROM FC36 to others. |
3/13/2025 8:36 AM | |
Joined: 2/21/2014 Last visit: 9/12/2025 Posts: 672 Rating:
|
Hello Willybong, I am sure that section list the FCs which are being called from the code of the block whose property is shown. It does not list what further calls the FCs being used in that code are making. |
You can always use "Rate" and "To Thank" button to appreciate my efforts in helping you :) |
|
This contribution was helpful to
1 thankful Users |
5/2/2025 7:26 AM | |
Joined: 2/11/2015 Last visit: 9/9/2025 Posts: 512 Rating:
|
Hi HarrY ji, Yes, you're right. So, if you click on FC36, left button, properties. you'll not see the call to FC36. |
Follow us on