7/22/2024 3:15 AM | |
Joined: 7/22/2024 Last visit: 7/22/2024 Posts: 1 Rating: (0) |
Hello, A word in advance: I created a new post, because it is about power supplies for CNC milling machine power amplifiers, and I haven't found any relevant information: I need a power supply for 5 stepper motor output stages, with an input voltage of 20-50V and an input current of 2A each (the stepper motors must provide 2.5A nominal current, the output stage produces 2A RMS and 2.83A peak). How can I choose the right one? Usually, power supplies have connections for 3 power amplifiers, so the other 2 power amplifiers must be connected in parallel with the others. I'm not sure how to calculate... If you have any questions about power amplifiers, you can find them here: https://www.oyostepper.com/goods-111-Digital-Stepper-Driver-10-42A-20-50VDC-for-Nema-17-23-24-Stepper-Motor.html
|
Follow us on