11/7/2022 2:23 PM | |
Joined: 2/17/2020 Last visit: 9/16/2025 Posts: 1251 Rating:
|
Hi, I would recommend you to use the following document as a guide for the conversion: Differences between the VB script functions of Windows and WinCE Another option would be to directly ask the developers of the application example through the 'Provide feedback' option at the end of the SIOS entry. |
A rating will be well appreciated. |
|
This contribution was helpful to
1 thankful Users |
11/11/2022 11:54 AM | |
Joined: 8/3/2009 Last visit: 9/17/2025 Posts: 16442 Rating:
|
Hello T.H.A the differences should be only in accessing the file system. Here you have an example how to use the Functinos for the file and filesystem access in a PC Runtime (not WinCE) https://support.industry.siemens.com/cs/ww/en/view/106501825 Bye Murof |
If this Information really helps, you could use the Rate function |
|
7/15/2025 10:08 AM | |
Joined: 10/29/2022 Last visit: 9/14/2025 Posts: 1 Rating:
|
Can you plz upload the sample project? That project is removed from the source. |
Follow us on