9/30/2013 12:54 PM | |
Posts: 1299 Rating:
|
Hello, you can find this in manual: https://www.automation.siemens.com/mdm/default.aspx?DocVersionId=39281800203&Language=en-US&TopicId=32139243787 Did youcheck your PG/PC-Interface in Control Panel? K!ke |
10/3/2013 12:06 PM | |
Posts: 45 Rating:
|
Dear Ricardo, What kind of explanation would you like to get from me? It is the most simple test program that I can imagine: - A button in the HMI sets the bit M10.0 when pressed, - when this bit is high, M10.1 becomes also high (one ladder PLC code line) - and the yellow figure on the HMI becomes visible if this M10.1 is high. I am using event: Press --> SetBit M10.0and Release --> ResetBit M10.0 Iknow that with Step7 V5.5 and WinCC flex 2008 I should not have any errors even if the code would be not good or HMI project not OK. It has to do with some interface / communication settings or something similar. The error text I have listed in my first pos, but anyway I attached all the screenshots you ask for: HMI , PLC and the error in one ZIP file. AttachmentHMI PLC Error.zip (1651 Downloads) |
10/4/2013 11:53 AM | |
Posts: 45 Rating:
|
Hoi Ricardo, I see ##### when I will read out some PLC data. Definitely there isno connection... |
10/4/2013 2:31 PM | |
Joined: 4/24/2006 Last visit: 9/15/2025 Posts: 9027 Rating:
|
Hello ASTECH, Great your problem is solved. Now I may wish you "a nice weekend". Best regards, Wizard |
10/4/2013 3:13 PM | |
Posts: 45 Rating:
|
Hallo, Yes, I'm also glad that it is solved. Have a nice weekend! |
Follow us on