10/27/2012 7:56 AM | |
Posts: 79 Rating: (7) |
Hello Patel Bhai Try to SET PG/PC from microwin, then you can see the microwin option. |
4/24/2013 2:39 PM | |
Joined: 1/25/2006 Last visit: 2/9/2023 Posts: 257 Rating: (60) |
We are here to help each other. BR.
|
This contribution was helpful to5 thankful Users |
8/23/2013 12:10 AM | |
Joined: 5/15/2007 Last visit: 2/21/2024 Posts: 14 Rating: (2) |
I installed first Microwin 4.0.8 (SP8) then Try install Microwin 4.0.9 (SP9) and the setup recommend me uninstall Microwin 4.0.8 (SP8), when the uninstall ended without windows restart, I try again install Microwin 4.0.9 and this ends succesfull Then I need to run this file (PCPPICable) for the PG/PC Interface show the <<Microwin -> PPI>> Inteface AttachmentPCPPIcable EjecutarParaIntefaceMicrowin.zip (4879 Downloads) |
Ivan Davila |
|
This contribution was helpful to4 thankful Users |
1/21/2014 1:48 PM | |
Posts: 340 Rating: (6) |
new question is splittet to PG/PC interface, trying to search for CPU, all three LEDs keep blinking |
3/25/2014 2:56 PM | |
Posts: 2 Rating: (2) |
Thank you sir, your script worked on my Windows 8.1 64bit, and no need to restart the computer. |
6/5/2014 9:24 AM | |
Posts: 1 Rating: (0) |
thanks for help!!! |
6/17/2014 2:52 PM | |
Joined: 3/25/2013 Last visit: 3/21/2019 Posts: 176 Rating: (1) |
New question split intoConnect to PLCs in Microwin on windows 8.1. With best regards, Narrator1
|
8/19/2014 4:05 PM | |
Posts: 1 Rating: (0) |
thank you very much this patch is very efficient with me ... i can recure my fault thank you again |
12/23/2014 12:50 PM | |
Posts: 4 Rating: (0) |
Thank youluciferC4, this patch works! I have installed Micro/WIN v4.0.9.25 on Windows 7 Ultimate SP1 64bit; Before patch I had error "specifies access point not found"
|
12/23/2014 2:14 PM | |
Joined: 1/25/2006 Last visit: 2/9/2023 Posts: 257 Rating: (60) |
You welcome! Best regards!!
|
4/24/2015 4:07 PM | |
Posts: 5225 Rating: (1187) |
Did you know... 2. |
Last edited by: William_B at: 4/24/2015 4:08:20 PM |
|
This contribution was helpful to1 thankful Users |
4/26/2015 5:23 PM | |
Posts: 1 Rating: (0) |
just starting MicroWin, Right Click it and 'Run as administrator'. Should work. |
5/23/2015 11:46 AM | |
Posts: 85 Rating: (0) |
Thank youluciferC4, this patch works! I have installed Micro/WIN v4.0.9.25 on Windows 7 Pro SP1 64bit; Before patch I had error "specifies access point not found"
Now it works fine ! Thank you so much ! |
9/21/2015 9:58 AM | |
Posts: 4 Rating: (0) |
This file also works for Win10 X64. Thank you very much for this tip!
|
10/7/2015 1:15 PM | |
Joined: 4/11/2015 Last visit: 5/11/2024 Posts: 14 Rating: (0) |
i want the patch but for win7 32bit |
11/16/2015 7:10 PM | |
Posts: 1 Rating: (0) |
Thanks it worked with me |
12/10/2015 9:58 AM | |
Posts: 1 Rating: (0) |
i have also same problem sanjay . |
9/19/2016 2:11 AM | |
Posts: 1 Rating: (0) |
i am trying to download the patch file it asks for a username and a password, How can i know my username and password ? |
1/13/2017 6:09 AM | |
Posts: 1 Rating: (0) |
Hello everyone, Is there a patch that works on windows 10 for the same issue? Thanks |
Last edited by: sagemlink at: 1/13/2017 6:09:55 AM |
|
4/24/2017 4:36 PM | |
Posts: 1 Rating: (0) |
Hello If one driver to send my friends. Driver for PC/PPI cable 6ES7 901-3CB30-0XA0Thank you
|
11/29/2017 9:59 PM | |
Posts: 439 Rating: (108) |
Hello, Thanks luciferC4, your patch solve an issue one of my customer had. He installed "STEP 7-Micro/WIN V4.0 SP6" which is not compatible with Windows 7. At this point he was not even able to uninstall "STEP 7-Micro/WIN V4.0 SP6" or to install/upgrade "STEP 7-Micro/WIN V4.0 SP9" (which is compatible with Windows 7) First thing: (This is what I found first, but did not solve all the issue) How do you uninstall STEP 7 Micro/WIN V4.0 after an aborted installation? Second thing: (This is what USA tech support gave me)
He was able to install "STEP 7-Micro/WIN V4.0 SP9" at this point. Then, he had issue with the Set PG/PC interface. He was not able to select "Micro/Win" in the "Access Point of the Application" list. I runned you .BAT file and it solved everything. Here is the contain of it:
Create a text file, copy/paste the above command in it and change the .txt to .bat and run it as administrator. I am now able to select "PC/PPI.cable.PPI.1" and also "Micro/Win". Thanks! Best regards, Hugo |
Last edited by: Jen_Moderator at: 11/30/2017 1:50:49 PMAdded picture as an attachment. |
|
This contribution was helpful to2 thankful Users |
3/25/2018 4:38 PM | |
Posts: 3 Rating: (0) |
Yes working good. Thanks you save,from lot of troubles |
4/19/2018 12:59 PM | |
Posts: 1 Rating: (0) |
Hi This patch works, I had been struggling for days with this problem and this patch solved my access issue. thanks for posting this kind regard Andy |
10/23/2019 7:06 PM | |
Joined: 1/30/2015 Last visit: 5/10/2024 Posts: 8 Rating: (0) |
I posted my solution for this issue in this post https://support.industry.siemens.com/tf/ww/en/posts/problem-instalation-of-microwin-v4-0/161414/?page=0&pageSize=10 Hope this helps someone. |
12/21/2019 1:08 AM | |
Posts: 1 Rating: (0) |
you saved me bro thanks a lot |
1/24/2020 4:46 PM | |
Joined: 7/18/2019 Last visit: 12/20/2022 Posts: 8 Rating: (0) |
With the microwin connection problem, use the mpi adapter and set the pc/pg interface as ppi cable. That works |
2/3/2020 7:34 AM | |
Joined: 12/29/2019 Last visit: 2/23/2024 Posts: 3 Rating: (0) |
This worked perfectly, thank you very much! |
3/12/2020 8:28 PM | |
Joined: 2/22/2020 Last visit: 4/26/2024 Posts: 1 Rating: (0) |
Thank you for your help and guidance I run the attachment and Micron 2 works well
|
12/17/2021 12:27 PM | |
Joined: 6/27/2016 Last visit: 7/7/2022 Posts: 1 Rating: (0) |
Thanks LuciferC4! The patch worked also on Win10 64bit! |
7/30/2022 1:31 PM | |
Joined: 3/16/2022 Last visit: 3/18/2024 Posts: 1 Rating: (0) |
Thanks LuciferC4!. WIN 7, 64BIT |
Follow us on