12/10/2017 9:39 AM | |
Posts: 22 Rating: (1) |
Now I got to work I missed that it but be in run mode to access webserver. Sorry IOX65 That I missed this.. Now I have to put a Summer/Winter switch that disable Q3 in Winter mode and enable in Summer mode. I also have to put a function that stop a pump when flow is not enough in pipe to get flow value I have a flow meter that send a analogue signal when flow is out of range. Also need put function for water meter that has M-bus sending signal with puls to calculate how much water is added in process. This must show day by day amount and total on month. I really not think my skills on logo 8 is enough to do this functions. You have interest to help me with this functions ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/11/2017 9:35:19 AMNew subject after splitting |
|
This contribution was helpful to1 thankful Users |
12/10/2017 10:02 AM | |
Posts: 22 Rating: (1) |
Is there some way to convert signal of the M-bus? This function is not prio. But all other is.. |
12/10/2017 10:13 AM | |
Posts: 22 Rating: (1) |
Okay I look in to this if find a converter. Can you please help me with other functions I feel it's above my knowledge in Logo? |
12/10/2017 10:22 AM | |
Posts: 22 Rating: (1) |
Aha I was mean a mechanical switch connected to logo. Like on/off Sorry maybe I do bad explaning |
12/12/2017 10:01 PM | |
Posts: 22 Rating: (1) |
Yes I mean a extern input. I tried but I can get this right (newbie) need help? When this input is active (1) it should disable out put Q3 and when not Active (0) it should enable Q3 again. Q3 should be disable even if temp. dropping if Input is active (1) I attached program AttachmentMed El patron.Standard).zip (298 Downloads) |
12/12/2017 10:15 PM | |
Joined: 12/18/2014 Last visit: 5/28/2024 Posts: 33119 Rating: (4089)
|
See attachment.
AttachmentMed El patron.Standard_V2.zip (310 Downloads) |
12/14/2017 4:30 AM | |
Posts: 22 Rating: (1) |
Sorry IXO65! 0 = Summer 1 = Winter |
12/14/2017 6:10 AM | |
Joined: 12/18/2014 Last visit: 5/28/2024 Posts: 33119 Rating: (4089)
|
Version 3.
AttachmentMed El patron.Standard_V3.zip (232 Downloads) |
12/14/2017 9:35 PM | |
Posts: 22 Rating: (1) |
Thanks work super. You are amazing IOX65. Now I start look for a M-bus to Modbus converters so I also can get use of water meter. Then project is finish. |
Follow us on