11/24/2010 5:02 PM | |
Posts: 20 Rating: (0) |
Hello everybody, I am new in the forum, but I have been working with simens instrumens. This time I want to talk about the BW500, the dyniamic weightmeter is working fine. I have a PI control into the PLC, so I am just using one analog output for flow. Recently We bought a MIT (moisture instrument), and I wanto to use this. According to the manual It is possible to use one analog input for this operation, but with the help of one extra I/O why? My questions is: I have two analog input built in with the BW500 that are doing nothing, Can I configure one analog input for this to use (MIT use)? Best Regards. hp Splitted from Milltronics BW500. |
Last edited by: O_Moderator at: 11/25/2010 11:38 AMnew subject after splitting |
|
Follow us on