4/6/2023 7:22 AM | |
Joined: 1/21/2013 Last visit: 9/12/2025 Posts: 4108 Rating:
|
Hi Danielchirita82, Are you using a fixed IP address for your engineering computer within the PLC subnet or are you using the temporary IP addresses from TIA Portal? If you are using temporary IP addresses, you may have an address conflict. You can try to delete the temporary address or reset the TCP/IP configuration. Kind regards |
4/6/2023 10:40 AM | |
Joined: 1/12/2023 Last visit: 5/13/2024 Posts: 19 Rating:
|
Thank you verry much Stefan Arcularius!!! I did it like you say. Now I can go online, and I can download software on both PLC and I can download Hardware just for PLC 254 but still I cannot download Hardware for PLC 253. About IP's, I use my laptop with IP LAN static and in Virtual Machine I use automatically adapter with bridge thru Laptop Network card. I try in many possibilities the IP configurations. I attached some captures. AttachmentCommunication 2 PLC.pdf (750 Downloads) |
4/7/2023 1:01 PM | |
Joined: 1/12/2023 Last visit: 5/13/2024 Posts: 19 Rating:
|
Dear Stefan, The IPs of Windows PLC Network Card was set automatically or manually without any success. Anyway, in final I try to download Hardware Configuration from Device View of PLC and was working perfect, now the links are kept for Download from anywhere. Also, this problem was post here with the approach issue I think: Connection problem - 124771 - Industry Support Siemens Thank you and best regards! AttachmentDownload Hardware Configuration for Communication 2 PLC.pdf (731 Downloads) |
Last edited by: Danielchirita82 at: 04/07/2023 13:02:47Last edited by: Danielchirita82 at: 04/07/2023 13:03:03 |
|
Follow us on