3/5/2024 11:12 AM | |
Joined: 2/17/2020 Last visit: 6/3/2024 Posts: 1008 Rating: (177) |
Hi, As the redundant connection of WinCC to S7-1500H was included in version V7.5 SP1, it would be interesting to install Update 5 and see if the behavior improves. Updates for WinCC V7.5 SP1 and WinCC V7.5 SP1 ASIA If the problem persists... - What is the version of SIMATIC NET installed? - Which access point has been selected in the PG/PC interface? |
A rating will be well appreciated. |
|
Follow us on