10/20/2016 10:46 AM | |
Posts: 45 Rating: (1) |
Hello WinCC experts. A client of mine has requested to create a daily report pdf of the operation status of some equipment and send this report via email. We are using WinCC 7.3 Depending of the status of the equipment the email will be sent to different accounts. For example, if motor is OK then send email to main account A@sample.com and CC:green@sample.com. If there’s a warning then send email to main account A@sample.com and CC:yellow@sample.com. If there’s a fault then send email to main account A@sample.com and CC:red@sample.com. I’ve attached a detailed description of what do I need to do (04-DAILY_REPORT.jpg, 05-DAILY_REPORT.pdf) and also some screenshots of my WinCC with the faceplates of motors and instruments. Additionally I would like to create a daily csv file of All Operation data and send it via email to a data storage account (data@sample.com). Also I would like to create a Daily export of all ALARMS csv file and send it via email to the same account. Any help on these topics will be appreciated. Thanks in advance. AttachmentDaily_Report.zip (258 Downloads) |
Last edited by: Antri at: 10/20/2016 10:47:15 AM |
|
3/21/2024 9:10 AM | |
Joined: 8/3/2009 Last visit: 6/10/2024 Posts: 12991 Rating: (1659)
|
Hello jthyge1 do you have TIA Portal also ? there is an example for sending Mails with a Script in WinCC Professional RT in the HMI Toolbox. I do not have testet it but WinCC Prof is very similar to WinCC V7/8. I would say this should also work similar in WinCC V7/8 https://support.industry.siemens.com/cs/de/en/view/106226404 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on