(0)| 4/3/2025 8:02 AM | |
|
Joined: 4/25/2015 Last visit: 12/27/2025 Posts: 115 Rating:
|
Hello, I wanted to try wincc unifed simulation after installing successfully the RT. Before I had to start PLCSIM which works fine on V18 and V19 but it didn't work on V20. I retried the installation which went trough the full installation without any error but I receive always the same message that the PLCSIM has no interfaces and moreover when I want to use it, the simulation starts the PLCSIM but doesn't start an instance. Even if I start manually an instance, I receive the same error message. If I start an instance, it's impossible to close this instance or to close the PLCSIM program. Any Idea what it could be? Best regards Claude ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 04/03/2025 08:42:08New subject after splitting Last edited by: Moderator_Lan at: 04/03/2025 10:59:56Title updated |
|
Follow us on