5/22/2022 3:09 PM | |
Joined: 5/5/2022 Last visit: 2/22/2023 Posts: 1 Rating: (0) |
(كيفية تثبيت SIMATIC STEP 7-Micro / WIN على نظام Win 10؟ لدي S7-200) المطلوب طريقة تسطيب البرنامج مثل كل البرامجاولا السلام عليكم. ثانيا ، أعتذر يا سيدي العزيز. سأحاول أن أترجم إلى الإنجليزية. المطلب الوحيد هو طريقة تركيب وتثبيت برنامج 200 داخل ويندوز 10 64 بايت ، مع جزيل الشكر والتقدير والاحترام.First, peace be upon you. Secondly, I apologize, my honorable sir. I will try to translate into English. What is required is only the method of installing and installing the 200 program within Windows 10 64 bytes and the programs that I request are only personal. -------------------------------------------------- ---------------------------------------- |
Last edited by: Jen_Moderator at: 05/23/2022 12:07:28New subject after splitting Last edited by: mounih at: 06/01/2022 13:08:38Last edited by: mounih at: 06/01/2022 13:10:27 |
|
5/22/2022 3:46 PM | |
Joined: 9/27/2006 Last visit: 10/17/2024 Posts: 12289 Rating: (2687) |
Hello Mounih; As you can see from this link, STEP7 MicroWIN V4.0 SP9 is the highest version that you can use, and it only runs up to Windows 7 (32/64 bit). https://support.industry.siemens.com/cs/ww/en/view/58523240 You really should consider a VM installation on your Win 10 PC, running Windows 7, and then you can run Microwin v4.0 SP9 with all functionalities. Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on