10/26/2021 3:31 PM | |
Posts: 3 Rating:
|
Hi, Is this script usefull for faceplates too? I want to alternate the visualization of the faceplate between two layers, using two buttons. I used the following script for one of the buttons:
Best Regards, Isabela. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/16/2021 13:26:22New subject after splitting |
|
10/27/2021 12:47 PM | |
Joined: 9/23/2005 Last visit: 9/10/2025 Posts: 4416 Rating:
|
Hi follow there is a sample project that works with faceplates AttachmentSampleProgra.zip (417 Downloads) |
Last edited by: Denilson Pegaia at: 10/27/2021 18:15:28Denilson Pegaia |
|
This contribution was helpful to
1 thankful Users |
10/28/2021 12:18 PM | |
Joined: 9/23/2005 Last visit: 9/10/2025 Posts: 4416 Rating:
|
Aditional TIP: using script on load screen/faceplate event, it is possible to hide some layer as default setting. Sample project AttachmentProject1_20211006_0859_20211027_0744_20211028_0711.zip (331 Downloads) |
Denilson Pegaia |
|
Follow us on