(1)| 9/25/2023 6:24 AM | |
|
Joined: 1/21/2013 Last visit: 1/19/2026 Posts: 4410 Rating:
|
Hi PrzemekELKAR, The solution you are using is based on the built-in PDF Viewer application. It is not possible to use the WinCC Unified GUI on a Unified Panel in parallel, since both applications only run in full-screen mode. However, you can use the Web Control instead. Kind regards |
This contribution was helpful to
|
|
| 9/25/2023 6:56 AM | |
|
Joined: 9/20/2023 Last visit: 1/24/2025 Posts: 8 Rating:
|
Hi Stefan,
Displaying PDF files in the "Browser" on a Unified Comfort PanelThe "Browser" object displays PDF files that are available:
You can view a PDF file in the following ways:
Syntax: file:///<path>/<filename>.pdf Pay attention to uppercase/lowercase spelling. Examples:
" But using syntax file:/// i get error: The value is invalid. URL has to start with 'https://' Is there a way to do this in TIa V17? Or is it only possible in TIA V18? |
Follow us on