10/16/2023 8:43 AM | |
Joined: 7/19/2022 Last visit: 9/15/2025 Posts: 436 Rating:
|
Hello AutoGen_4123457, You can make a small script on the basic image with "Alternate Background Color" calls the alarm popup when the signal becomes "true". See attached image. As an alternative and possibly better solution, in WinCC Unified Toolbox there is an example of how to display an indicator (e.g. a red light symbol) when there are pending alarms. For example, you can also run this indicator as a button to open an alarm popup. |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on