(4)| 10/30/2023 11:27 AM | |
|
Joined: 1/20/2022 Last visit: 9/3/2025 Posts: 369 Rating:
|
Do these SD cards not come pre-formatted from siemens? So if its FAT32 or NTFS then it has to stay in this format? Is NTFS more prefered for consistency of the files? Regards
|
| 10/30/2023 11:50 AM | |
|
Joined: 1/21/2013 Last visit: 1/17/2026 Posts: 4406 Rating:
|
Hi hewking103,
Yes, and this is probably true for all other manufacturers as well.
No, you can format it. However, because the 32GB card can be used as a system memory card - which requires special formatting - if you format such a card, it will no longer be usable as a system memory card, but you can use it as a data memory card.
You may have noticed that I try to include links to additional information in my posts. In the 'Connecting a USB device' chapter you will find: We recommend using the "NTFS" formatting method which offers greater data consistency and flexibility regarding the size of the saved files. Kind regards |
| 10/30/2023 11:59 AM | |
|
Joined: 1/20/2022 Last visit: 9/3/2025 Posts: 369 Rating:
|
sorry i try to open all links you sent but missed that one its all clear regarding the sd Cards!
|
This contribution was helpful to
|
|
Follow us on