(0)| 10/18/2024 12:11 PM | |
|
Joined: 8/3/2009 Last visit: 1/21/2026 Posts: 16653 Rating:
|
Hello jdez I tested it with TIA V19 Upd3 and it works: -> i guess you do not have installed the Upd3 for WinCC Unified PC RT -> its available now: https://support.industry.siemens.com/cs/de/en/view/109820989 Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
| 10/18/2024 6:05 PM | |
|
Joined: 1/21/2013 Last visit: 1/21/2026 Posts: 4424 Rating:
|
Hi jdez, Providing more details about your system would make it easier to answer. When you created the post, V19 Update 3 was only released for the WinCC Unified Engineering System. For the devices (PC Runtime, Comfort and Basic Panel) the update was released on October 15th. However, since I have to guess, I would say that you are using a WinCC Unified Comfort Panel with image version V19.0.0.2. I know that there is a problem that the Trend Companion does not use the colors like the PC Runtime. However, I am afraid that this behavior is not yet fixed with Update 3. Kind regards |
| 10/21/2024 6:59 AM | |
|
Joined: 11/30/2018 Last visit: 1/21/2026 Posts: 59 Rating:
|
Support may have sent us an update earlier due to a completely different problem. Correct, the behavior is not fixed yet. I made a simple color legend on the side and moved on. |
Last edited by: jdez at: 10/21/2024 07:20:20 |
|
Follow us on