(0)| 12/2/2024 3:36 PM | |
|
Joined: 2/17/2020 Last visit: 1/9/2026 Posts: 1251 Rating:
|
Hi, The System Alarm with ID "536870921" in Unified Panels means that the connection to the Service Manager has been lost: Unified manual > Runtime system eventsI believe this can occur if: => a not suitable USB device on X61/X62 is used for the Tag Logging or Alarm Logging database. => behavior is also triggered when you use a SD Card and the card is write-protected. |
|
A rating will be well appreciated. |
|
| 12/6/2024 10:34 AM | |
|
Joined: 8/3/2009 Last visit: 1/9/2026 Posts: 16629 Rating:
|
Hello Maris777 you could use an alarm subscription... For example there is an alarm indicator example in the Toolbox. This subscription you should be able to use to react on any incoming alarm https://support.industry.siemens.com/cs/de/en/view/109770480 Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on