(0)| 3/17/2025 5:07 PM | |
|
Joined: 11/28/2024 Last visit: 6/15/2025 Posts: 43 Rating:
|
Hi, What is the script function for border width? |
Last edited by: AutoGen_12877 at: 06/15/2025 21:12:28 |
|
| 3/17/2025 9:22 PM | |
|
Joined: 1/21/2013 Last visit: 1/23/2026 Posts: 4427 Rating:
|
Hi, The polygon property that represents the with is the "Width" property, as for all other elements with such functionality. Note that it is of type UInt32, so depending on your text it can be 2 or 3, nothing in between. However, when you dynamize a property, you do not need the name of the property because the dynamization script must return a value. So within the dynamization script function, program whatever you want and make sure that 2 or 3 is returned. Kind regards |
| 3/18/2025 12:08 PM | |
|
Joined: 11/28/2024 Last visit: 6/15/2025 Posts: 43 Rating:
|
ok |
Last edited by: AutoGen_12877 at: 06/15/2025 21:13:04 |
|
Follow us on