(0)| 5/9/2012 3:20 PM | |
|
Joined: 8/25/2006 Last visit: 1/21/2026 Posts: 2221 Rating:
|
Hello. All connectors in the drive are represented in % of rated value. You may read about normalization of each connector in themanual, chapter 12. For configuring analog inputs/outputs there are special normalization parameters, e.g. P701 for AI at terminals X174:4,5 or P711 for AI at terminals X174:6,7. The same are available for analog outputs (e.g. P721, P731). Look at manual, function diagram sheets G113-G116, chapter 8. For the power I could find only K0307 - motor power output (Normalization:16384 =∧P100 * (P101 – P100 * P110)). |
Follow us on