(0)| 9/5/2014 9:14 AM | |
|
Joined: 10/11/2006 Last visit: 12/22/2025 Posts: 6062 Rating:
|
Hello Capraloris, as Masterdrives products arephased out(http://support.automation.siemens.com/WW/view/en/44011534) and are only available for spare part, you need to change over to SINAMICS. For SINAMICS no Simolink communication is available, so you need to use profibus communication or SINAMICS Link, which is similar to Simolink designed as communication interface between drives (SINAMICS AC inverters with CU320-2 (e.g. S120)and SINAMICS DCM with CUD Advanced). So when changing to SINAMICS AC, we would recommend to upgrade also from Simoreg to SINAMICS DCM. |
|
With best regards, |
|
Follow us on