(0)| 8/21/2017 11:22 AM | |
|
Posts: 1 Rating:
|
Hi all! I have a old servo motor with name plate: 1FK7042-5AK71-1KH3-Z with Z:X01 as image, which is encoder is AM16DQ K30. I buy a new servo motor with name plate: FK7042-5AK71-1KH3-Z with Z:X01 as image, which is encoder is AM16DQ K60. Two motors have the same nameplate, encoder type and difference only in K30, K60. Now, I can't replace the motor. I don't know the K30, K60 which mean.
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/22/2017 12:44:06 PMNew subject after splitting |
|
| 6/7/2018 12:30 PM | |
|
Joined: 10/11/2006 Last visit: 1/21/2026 Posts: 6052 Rating:
|
Hello, if the acknoledegment of the changed serial number does not solve your problem, we recommend to contact the technical support and provide the project and all fault messages to them: Support Request: https://support.industry.siemens.com/my/ww/en/requests/#createRequest |
|
With best regards, |
|
Follow us on