1/30/2019 3:12 PM | |
Posts: 2826 Rating:
|
Yeah, I get the namings Siemens use wrong. But yes I was thinking of the modes in the MC_HOME block. A reminder is attached as a PDF. You have several options there to look at. > My sensor is always the same for referencing. These two statements contradict each other. Would you care to explain? Keep in mind that configuring an input to be linked with the motion control, does not mean it cannot be used in normal code. Defining a profile for homing, does not mean you have to use homing. Active homing will work well for you. Passive homing will need you to code the movement, but the referencing ("zeroing") happens in the background when triggered. AttachmentMC_HOMING.pdf (515 Downloads) |
1/30/2019 3:46 PM | |
Posts: 2826 Rating:
|
(more info) |
Follow us on