9/3/2019 5:09 PM | |
Joined: 3/9/2018 Last visit: 8/31/2024 Posts: 189 Rating: (14) |
I finally got this module and got this error to when i used the Ethernet wizard. Didn't take me long to figure out I needed to use the Internet wizard as PLC information pointed out the 242-1EX01 is a internet module. The wizard is a bit misleading, because it allows you to select the 1EX01 is both wizard. /edit also pointed out in the 243-1 manual "Use the Internet wizard of STEP 7 Micro/WIN 32 to program communication in the user program (see chapters Configuration (Page 43) and Programming (Page 81)." AttachmentFiles.zip (177 Downloads) |
Last edited by: Henry1675 at: 09/03/2019 17:39:43Last edited by: Henry1675 at: 09/03/2019 17:52:59Last edited by: Henry1675 at: 09/03/2019 17:54:45Last edited by: Henry1675 at: 09/03/2019 17:55:48Last edited by: Jen_Moderator at: 09/04/2019 10:18:44Added pdf and jpg file as an zip file. |
|
This contribution was helpful to1 thankful Users |
9/4/2019 12:14 PM | |
Joined: 11/16/2016 Last visit: 6/23/2022 Posts: 45 Rating: (1) |
thanks |
Follow us on