12/10/2020 8:23 PM | |
Joined: 9/23/2005 Last visit: 9/10/2025 Posts: 4416 Rating:
|
Hi, “Simple Samples” are small projects that demonstrate simple features. The target is giving a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. Switches are simple elements that allow the operator to alternately assign one of two values (e.g. true or false) to a variable. In addition to the assignment, it also clearly represents the status of this variable. Configuration: The assignment of values to the switch is done in the General -> Alternative state property. Tips:
Project (archived and zipped) AttachmentSwitch.zip (1171 Downloads) |
Denilson Pegaia |
|
12/10/2020 8:26 PM |
|
Joined: 12/27/2018 Last visit: 10/2/2024 Posts: 510 Rating:
|
Hello Denilson Pegaia Are you alive in the forum? |
Jinson James, M.Tech (Power Electronics and Power System), |
|
Follow us on