12/29/2020 11:13 AM | |
Joined: 9/23/2005 Last visit: 9/10/2025 Posts: 4416 Rating:
|
Hi, “Simple Samples” are small projects that demonstrate simple features. The target is giving a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. In general, there are two main alarm/message types:
An additional type of alarm/message type are the generated by the user / operator: e.g. it report process event that are not covered by the other types, done by the user and that should be registered, like for example, turn shifts, changing production orders, report visual abnormalities of production, noises, etc. Operator / User Alarms / messages could be generated by system functions / scripts. There are three available system functions:
TIPs:
Attached there is an example project (archived and zipped). Attachmentproject.zip (1389 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
2 thankful Users |
Follow us on