2/20/2024 6:08 AM | |
Joined: 1/21/2013 Last visit: 9/12/2025 Posts: 4108 Rating:
|
Hi Kassidy, You can look at the 'SIMATIC Runtime Manager' and check if it takes up to 2 minutes to reach the 'Running' state. If it takes that long, a deeper analysis would be necessary. The first step would be to use the Trace Viewer. But analyzing these logs can be a very hard job. So it might be better to contact technical support instead. Kind regards |
2/20/2024 6:49 AM | |
Joined: 3/15/2019 Last visit: 9/12/2025 Posts: 16 Rating:
|
Hello friend, check if the browser has not set a proxy |
2/23/2024 9:56 AM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello Kassidy do you have set up your Runtime/Engineering system properly: https://support.industry.siemens.com/cs/de/en/view/109806850 does it work only that long in one specific project or every time you use the simulation/runtime? Which Update do you have installed in engineering and for the Unified Runtime? Bye Murof |
If this Information really helps, you could use the Rate function |
|
6/8/2024 9:53 AM | |
Joined: 3/15/2015 Last visit: 5/26/2025 Posts: 15 Rating:
|
Any Updates? i have same problem.. |
Follow us on