8/1/2017 1:56 PM | |
Joined: 4/16/2015 Last visit: 4/3/2024 Posts: 45 Rating:
|
Dear community, As the IOT2000 community is growing rapidly through your participation we want to say: Thank you! To even expand the IOT-Community further we love to have your feedback on the device and share success stories of you using the IOT2000 in most different ways. Those stories and applications could then be published in the IOT2000 Forum or in our online reference center Your application could have a remarkable impact for users and customers to come! What is your benefit?
Interested to make a contribution to the IOT2000 Community? |
Last edited by: Philipp_ at: 8/1/2017 8:59:05 PM |
|
This contribution was helpful to
2 thankful Users |
9/23/2017 7:24 PM | |||
Joined: 6/14/2016 Last visit: 4/24/2024 Posts: 1 Rating:
|
IOT2020 (Private and Education Focus): Private Person IOT a la maison, Edition II
What is the role of the IOT2000 in your Project? Monitoring the data from 4 temperature sensors (PT100) located at Hot-Water-Tank*), and use the evaluated data via web through WLAN to optimize the combination of heating process. *) Note: Energy provide viatiled stove with water bag, solar cell and oil heating system. Why did you choose the IOT2000 for your Project? Same solution was realized by me with Arduino board and programmed with Arduino IDE last Year. However, I want to upgrade that "Hobby" IOT solution (Edition I) to industry IOT solution (Edition II), This application was written in Arduino IDE and Node-Red. (Upate: Feb. 2020) 2) With this change, more sensors (like Level measurement of Heating Oil) are added and addtional Visualizsations are created at the iobroker Server. 3) The advantage of this solution: No Change at Simatic IOT 2000, all data are keeped at my Home Server, no Cloud is needed ! (Update: Feb. 2020) New: (Feb. 2021) (Update: Dez. 2023) This Solution applied with SIMATIC IOT2000 works since 2019 without any problem till now. How did you find oLevel measurementut about the IOT2000? It was introduced at a Siemens conference November 2016 AttachmentNeu IOT Messung am Pufferspeicher.pdf (1976 Downloads) |
||
Last edited by: SICAR at: 02/02/2020 17:26:35Last edited by: SICAR at: 02/10/2020 10:43:04Last edited by: SICAR at: 02/11/2021 21:47:46Last edited by: SICAR at: 02/12/2022 17:15:30Last edited by: SICAR at: 12/02/2023 10:29:47 |
|||
This contribution was helpful to
12 thankful Users |
10/23/2017 11:48 AM | |
Joined: 3/17/2014 Last visit: 1/15/2024 Posts: 53 Rating:
|
Hi, as technical sales referent here in Italy for IOT, I would publish one of our success story in behalf of one customer of us. Company Name? Sage Srl Company Type? OEM Machine Types? Converting - Slitters and rewinder What is the role of the IOT2040 in your project? IOT2040 as a Gateway for Industry 4.0 IOT connected to an S7.300 and fully programmed with Node-RED. Main features below:
Why did you chose the IOT2040 for your project? Linux Envroinment - Low Price - Lot of function can be implemented AttachmentSage_Images.zip (2368 Downloads) |
This contribution was helpful to
4 thankful Users |
12/16/2017 2:55 PM | |
Joined: 2/2/2017 Last visit: 4/27/2024 Posts: 36 Rating:
|
Company Name? Crickets Automation
Company Type? ISV Machine Types? General purpose What is the role of the IOT2040 in your project? IOT2040 as a WebHmi/scada and Gateway for Industry 4.0 and IOT Crickets Automation has developed the first standard software for IOT2000 platform. xvisionIOT is a general purpose WebHmi/scada embedded into IOT2040. A new generation of intelligent objects that are always connected. Main features below:
New! imports tags from TIA portal (using TIA Portal openness) New! MS Azure connector New! Modbus Tcp slave connector New! OPC UA server connector Why did you choose the IOT2040 for your project? World wide availability - CE and UL compliance - serial and ethernet ports - low cost industrial hw & sw solution. AttachmentxvisionIOT_images.zip (2265 Downloads) |
Last edited by: cri2017 at: 12/16/2017 2:56:23 PMLast edited by: cri2017 at: 12/16/2017 5:01:20 PMLast edited by: cri2017 at: 10/29/2019 15:22:53 |
|
This contribution was helpful to
11 thankful Users |
3/3/2018 8:10 PM | |
Posts: 5 Rating:
|
Small Energy measurement equipment for monitoring a machines power consumption to 63 Amps Siemens IOT 2040 with PAC 2200 The PAC 2200 energy measurement device is connected via serial Modbus to the IOT. The measured values is published to the web page and connected to a SQL database (V2 version). The IOT is programmed with Node-red. The Pac device is using float dataformat , we wrote a function to convert the two 16 bites word to float. AttachmentIOTwithPAC2200.zip (1962 Downloads) |
Last edited by: Bzs at: 3/3/2018 8:10:45 PM |
|
This contribution was helpful to
5 thankful Users |
Follow us on