(0)| 4/24/2023 4:38 PM | |
|
Joined: 1/13/2022 Last visit: 12/4/2024 Posts: 1 Rating:
|
hello how are you I have a question I have an encoder in a production line which I want to replace since it is damaged but when connecting it sends me error F07955 the two encoders are the same they match in the code 6FX is a device from the s120 family later I connected through scout and extracted the data and it gave me a different motor I don't know if the encoder is the wrong one or it has a chip in the servo that tells it which servo it is or only the encoder has it please if you can help me since I need mount it to the production line. the two encoders match in the 6FX2001-3JC22-3DA0 Or do they have to match another encoder code? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/25/2023 08:49:52New subject after splitting |
|
Follow us on