(0)| 9/21/2024 8:04 PM | |
|
Posts: 2 Rating:
|
I do the same in my s120drive system which Consisting of one SLM and two control Unit and PLC1500T and 8 Servo motors in my case I need to get the enable operation signal from SLM which connected with first control Unit & the motors1&2&3&4 via drive CliQ to the second control unit motors 5&6&7&8modules with the aid of PLC logic but the problem with me is the SLM (Telegram 371) tags dose not appears on plc Default table tag however, the Motor modules tags appear (I think because the motor modules called by the PositioningAxis TO) So, how may I solve this problem? ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_1862864 at: 09/21/2024 20:07:03Last edited by: Moderator_Lan at: 09/23/2024 08:25:27New subject after splitting |
|
Follow us on