(0)| 1/14/2026 1:41 PM | |
|
Joined: 1/21/2025 Last visit: 1/14/2026 Posts: 2 Rating:
|
Hello, I am trying to set up a commusnicaton between Bender iso415r When I run my Modbus_Comm_Load I get no error, only state 16#0000 And Done Then when I try to read with Modbus_Master from address 1000 and length 1, I get the error 16#80C8. So also according the mentioned post, There is an issue in the G2 or the CB 1241. |
Last edited by: AutoGen_1866723 at: 01/14/2026 13:43:05Just a little change of line breaks for better readability. Last edited by: AutoGen_1866723 at: 01/14/2026 13:45:56Removed images, they were scaled down and unreadable. |
|
| 1/14/2026 2:03 PM | |
|
Joined: 7/31/2020 Last visit: 1/14/2026 Posts: 474 Rating:
|
Hello, The linked page indicates that the firmware can be updated using the Automation Tool. Required user action:
Best regards |
This contribution was helpful to
|
|
Follow us on