(0)| 3/30/2009 2:41 PM | |
|
Joined: 5/28/2008 Last visit: 9/1/2025 Posts: 901 Rating:
|
Hello, your problem is your Panel. The TP 170 could only 1 connection. thats the reason why protool say that there is no driver. you have to choose another panel which could project more connections. here is a list: http://support.automation.siemens.com/WW/view/en/15363798 regards manfred |
| 3/30/2009 3:16 PM | |
|
Joined: 5/28/2008 Last visit: 9/1/2025 Posts: 901 Rating:
|
sorry maybe i wrote it wrong.. |
| 3/30/2009 3:22 PM | |
|
Posts: 3 Rating:
|
thx, i will try to get my data directly from the S5 without using the TP grtz, stine |
| 9/30/2009 7:44 PM | |
|
Posts: 26 Rating:
|
Hi lads, i think I'M having the same problem I had an OP17 with CPU 928. Now I had to change from 928 to 948. I changed the features of the cpu in the protool project from 928 to 948 but I still get the same error "there is no driver ...." Whant can be the problem? Errors I get: $040 NO PLC and $115 RESTARTING PLC In the manual of the OP17 i can read: $115:stablishment of logical link with PLC in progress..... Have the PLC to be off while this? |
Follow us on